SICK Sensor Blog

SICK Sensor Blog
SICK Sensor Blog

Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.

Filter articles

653 results:

Result 577 - 600 out of 653

Counting impulses and detecting changes in speed one step earlier based on acceleration - this combination unprecedented on the market is provided by the SAM inductive proximity sensor from SICK. ... Read on
South Africas largest electricity producer ESKOM has set itself a significant task: to continuously monitor its dust concentration levels and, at the same time, meet the requirements stipulated by the... Read on
For cleaning subway tunnels, the special equipment supplier Schörling has developed a self-propelled train, equipping it with intelligent sensor technology from SICK. In dark tunnels, this technology... Read on
When commissioning a production order in the production department, e.g. final assembly or engine production in the automotive industry, then various sub-quantities may have to be put together from the... Read on
Highways and other busy traffic routes are dangerous obstacles for animals living in the wild. Green bridges (wildlife crossings) connect the animals habitats. Roe deer, red deer, wild boars, and... Read on
Itella, the Finnish mail and communication company (formerly Finnish Post), has invested in new sorting and detection systems at several parcel sorting centers. As a first in this sector, combined... Read on
The Jiangsu Sha Steel Group is the largest private steel group in the Peoples Republic of China. For detection of oil and water pressures PBS pressure switches are being used. The transmitter, pressure... Read on
As the trend towards ever more powerful machines continues, ways of protecting them are also in need of constant development. Safe movement monitoring helps to keep risks to a minimum, as it not only enables... Read on
For a long time, it was a critical moment to both passengers and streetcar personnel when the doors of the Cobra series of streetcars in Zurich were closing. These vehicles featured a photoelectric sensor... Read on
Equipping adjacent machines with only one safety component is extremely economical. In the context of the Scanner Plus! campaign, SICK has adopted this approach as a mission, developing the Sim-4-Safety... Read on
Efficient flue gas cleaning is used in modern power stations. A secondary method used to reduce NOx is the SCR (selective catalytic reduction). Thanks to the unique SCR Bypass System from SICK, modern... Read on
Who does not know the endless lines at the baggage counter of an airport? But help is on its way. Just as you can scan your own items at the supermarket today, it will be possible in future to check in... Read on
WTB12-3 Line photoelectric proximity sensors from SICK ensure 100-percent counting reliability in the counting and weighing machines for baked goods made by A&B Verpackungsmaschinen Manufaktur GmbH... Read on
Safety for automated guided vehicles on all paths and in all direction, combined with economic efficiency - this specification from the Spanish intralogistics provider ASTI is fulfilled by complete protection... Read on
In the context of plant modernizations, the Belgian French fries producer Lutosa cooperated with SICK to implement an intelligent concept at the plant in Leuze-en-Hainaut that provides maximum machine... Read on
Productivity of a machine is the key to efficient automation. Smart Sensor Solutions powered by IO-Link ensure consistency in automation networks, thus opening up potential for effective application solutions... Read on
The new MPA from SICK is the versatile solution for linear distance measurement and position detection of pistons in pneumatic drives. The analog positioning sensor delivers convincing performance due... Read on
More than 25,000 drivers decide each day to use the Liefkenshoektunnel. By doing so, they avoid traffic jams that often form on Ring 1 around Antwerp, Belgium. Today, the tunnel is the only toll road in... Read on
Using the function blocks specifically developed for integration of the AFS60 and AFM60 EtherNet/IP encoders into Rockwell controllers allows retrieving, reading, and partly writing (set and get) pre-installed... Read on
Navigating through interactive contents by movements of the hand like Tom Cruise in Minority Report - this is the dream that the Swiss Atracsys company has made a reality with the beMerlin LV. The LMS100... Read on
Hoisting walls are installations for lifting and lowering stage sets. In this connection, it is essential that the required path and position data be detected with great precision. ATM60 SSI absolute encoders... Read on
Anyone who believes to be part of the action in a 3D movie is well-advised to experience 4D cinema technology. Mobile cinema seats cause gravitational and centrifugal forces, among others, to impact the... Read on
Laser detectors from SICK already protect many museums, banks, public institutions, penitentiaries, and other important buildings. For these systems trigger alarm signals before break-ins can occur in... Read on
Safe and fast Internet connections, tamper-proof authentication methods, as well as intelligent sensors and controllers are the foundation of SICK Remote Services - the new service range offered for individual... Read on

Result 577 - 600 out of 653