SICK Sensor Blog

SICK Sensor Blog
SICK Sensor Blog

Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.

Filter articles

653 results:

Result 529 - 552 out of 653

SICK's reliable and user-friendly W11-2 and W4-3 photoelectric sensors help Swiss trading company Avesco AG to provide a fast delivery service for construction machinery components. SICK's photoelectric... Read on
ARBURG is a global leader in the manufacture of high-quality injection molding machines. The company was searching for a solution that would identify incorrectly positioned inserts, preventing the production... Read on
The French regional transport operator RATP has completed a project investigating the rolling characteristics of its regional trains. The aim of the project was to identify rail wear zones in order to... Read on
Actemium Logistics provides automated solutions such as picking, conveying and sorting, WMS integration for companies working in logistics. As a means of securing access to a palletizing system for E... Read on
Drivers are familiar with winding around annoying curves in the parking garage until finally sighting an open spot. If the driver has a plane or train to catch, this can be especially unpleasant. This... Read on
From laser-based bar code scanners and high-end solutions with 2D cameras to RFID technology: SICK is synonymous with years of know-how and experience in all automatic identification technologies. This... Read on
Every year in the Swiss Alps you can hear the sound of debris flows with thousands of tonnes of detritus rushing down into valleys, and towards endangered transportation routes and settlements. The Swiss... Read on
The Tele2 Arena in Stockholm is a stadium with a retractable roof. The benefit for spectators in the stadium and television viewers: There are no shadows on the playing field, when the roof is fully... Read on
Measuring the oxygen in the process can be quite simple. The TRANSIC100LP from SICK is the rugged transmitter that uses Tunable Diode Laser Spectroscopy (TDLS) to measure O2 reliably. A technology more... Read on
Clothes make the man, so says the proverb - but only if they fit. Despite the vast number of available sizes, it is sometimes difficult to find a shirt, pants, a dress or a skirt that fits perfectly. Custom-made... Read on
Frozen fish specialties are a solid alternative to fresh fish.  But where was the fish caught? And how?  Femeg, a German producer of frozen fish specialties, has the answer: QR codes on frozen... Read on
The Chinese railroad network carries an average of 42 million passengers every year, making it the world's busiest transportation service. In the past, rockfalls and debris avalanches falling onto the... Read on
Every year more than a million fall accidents are registered per year.The medical product developer BAAT Medical has built a unique fall simulator, which is equipped with safety components from SICK,... Read on
The deTec2 Core safety light curtain from SICK represents yet another feat in the new deTec device generation. After launching the deTec4 Core, which is certified for PL e or SIL3, last year, the sensor... Read on
The new Lector620 OCR image-based code reader is the ideal solution for reading and identifying printed plain text in packaging applications. Lector620 OCR reads best-before dates and batch numbers,... Read on
Optimalog was founded in 2006 and develops specialized automation software for PCs. They are currently developing a robot that can fully automatically cultivate an agricultural research park for the French... Read on
Solvents are used e.g. in paint shops and coating lines and being disposed in exhaust air decontamination systems. This process creates gas mixtures, the concentration of which must be analyzed to prevent... Read on
To maintain clean air, harmful emissions such as waste gases or dusts must be qualitatively and quantitatively recorded and kept to an absolute minimum. As the only provider of in-situ measurement technology... Read on
When public and industrial buildings or private houses need to be secured against intrusions, jailbreak, theft, vandalism or terrorism, structural measures or protection by security guards often... Read on
There is not a farmer in sight in the Van Aart family's barn. Yet the cows are still standing in line to be milked. Ever since the two MR-S1 milking robots arrived from BouMatic Robotics in Emmeloord,... Read on
Even things not graspable are now detected reliably: Infrablack object with only 1 % diffuse light reflection can be detected dependably at a range of up to 50 mm. Innovative technologies constitute... Read on
Assan Hanil is one of the leading automobile suppliers in Turkey. The company produces automotive accessories in its 30,000 m2 factory. For the protection of personnel in the paint shop's hazardous area... Read on
A flexible system for hazardous area protection on tire curing machines ensures optimum safety, efficiency, and ergonomics for the tire manufacturer Continental. As part of an international project,... Read on
Reliably detecting transparent items in translucent pack­ages - at B. Braun, manufacturer of medical products, the Inspector I40LUT vision sensor manages what conventional image-processing solutions... Read on

Result 529 - 552 out of 653