SICK Sensor Blog

SICK Sensor Blog
SICK Sensor Blog

Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.

Filter articles

653 results:

Result 409 - 432 out of 653

Virtually all system operators need to operate machines efficiently even when batch sizes are small, when products and formats need to be changed frequently, or when packaging varies in terms of design... Read on
Consistent quality, very few rejects, reliable part and batch tracking, added transparency: The use of vision sensors for quality control directly in the production process offers a number of benefits... Read on
scanware electronic GmbH in Bickenbach, Germany, develops and manufactures inspection systems for the 3D quality control of pharmaceutical products during the packing process. Nowadays, 2D cameras are... Read on
Rising passenger figures are a major challenge for airlines, ground handlers, and baggage handling system operators. After all, more passengers also means more baggage which has to be logged, sorted, and... Read on
Manufacturing a tire requires over one hundred individual steps and a wide array of components - a complex process with high standards when it comes to quality and safety. Careful testing is absolutely... Read on
Icelandic company Marel is the worlds leading provider of advanced food processing solutions for the fish, meat, and poultry industries. These solutions are provided in the form of modern equipment,... Read on
In 2015, the young Danish company Mobile Industrial Robots (MiR) introduced the German market to the MiR100, a mobile transport robot that works like clockwork. Built-in S300 safety laser scanners, 3D... Read on
In the factory of the future, humans and robots will collaborate to an increasing extent. Based on this vision, RoboJob develops innovative systems for the automated loading of machine tools. Safety laser... Read on
The new Dx1000 long range distance sensor from SICK features extreme versatility in any application and enables distance measurements with high measurement reliability, even in the presence of ambient... Read on
The continuous condition monitoring of electrical drives is growing in prominence. This is because the purely digital HIPERFACE DSL® interface makes it possible to provide status data such as the temperature... Read on
In the last few years, the furniture manufacturing industry has started to move away from largely supply-oriented toward demand- oriented production. This presents two challenges to manufacturers of woodworking... Read on
An increasing number of digital solutions are also being used in the fashion and clothing industries. The opportunities range from labeling products and presentations in stores all the way through to interaction... Read on
Since the end of 2013, the new global standard EN ISO 14119 (Safety of machinery - Interlocking devices associated with guards - Principles for design and selection) has been taking the place of the former... Read on
After water, tea is the worlds most consumed beverage. More than three billion cups are drunk each year in countries across the globe - the equivalent of around 450 cups per person in a year. As a beverage,... Read on
A wide range of industrial applications in nearly all industries can be covered with 3D vision sensors. While 2D vision sensors only measure the x- and y-axes of an object, 3D vision sensors are also designed... Read on
The impending updates to the BREF documents have indicated that mercury emissions from large combustion plants will soon have to be reduced dramatically. However, a reliable measurement solution is already... Read on
A sensory check can mean two things in the context of ice cream. Namely, the sensual experience of the chocolate coating cracking as you bite into it, followed by the explosion of flavors. Or it can refer... Read on
The Langenthal-based company Nencki AG is very meticulous when it comes to their bogie test stands. By using BTF08 HighLine wire draw encoders with an EtherCAT® interface and OD displacement measurement... Read on
Counterfeit pharmaceuticals cause major financial losses, can pose health risks, and undermine patients trust. In light of this, the pharmaceuticals industry has committed itself to implementing the EU... Read on
When it comes to metal closures in packaging, nothing can be left to chance: In products such as jam jars, the consumer goods industry requires seals to be tight and jars to be hermetically sealed. Anyone... Read on
Thanks to the PSDI (Presence Sensing Device Initiation) function in the Flexi Soft safety controller, it is possible to control the press cycle in manual insertion presses using a type 4 safety light curtain... Read on
One of the major issues associated with Industry 4.0 is making workflows flexible and that includes closer interaction between humans and machines. Part of this current move toward more integrated working... Read on
At the test labs in one of the worlds largest and most cutting-edge dishwasher factories, BSH Hausgeräte GmbH has invested in a fully automated robot to conduct lifecycle tests on dishwasher panels... Read on
 FLOWSIC600-XT - the new gas flow meter from SICK seamlessly preserves its predecessors positive image as an outstanding precision measurement device for demanding industrial environments. The FLOWSIC600-XT... Read on

Result 409 - 432 out of 653