The SPEETEC® is a sensor solution for moving materials in a linear path and special processes
SICK LAUNCHES NEW PRODUCT FOR NON-CONTACT MEASUREMENT OF SPEED AND LENGTH
Oct 13, 2020
MINNEAPOLIS, MINN., OCTOBER 13, 2020 – With the SPEETEC®, SICK is expanding its product range for speed and length measurement of objects moving in a linear path to include technology that measures directly on the material surface. The non-contact sensor is able to measure a wide range of web and continuous materials, as well as blanks with an accuracy of just 4 μm.
From a market perspective, the speed sensor closes the gap between tactile, indirect-measuring encoder solutions and laser velocimeters, which are often expensive to purchase and require considerable effort to integrate and operate.
Slip-resistant, without measuring elements, without damaging sensitive surfaces and without wear and tear on tactile sensor elements – the SPEETEC® from SICK is an innovative, non-contact sensor for speed and length measurement of objects moving in a linear path.
Look, but don’t touch: The sensor for special materials
For sensitive, soft, or smooth surfaces, customers from factory or logistics automation require non-contact measurement options for the length, speed, and position of continuous webs and blanks. Optical scanning prevents damage or contamination, thereby increasing product quality.
The SPEETEC® offers a new way to measure without slip, measuring elements or marking, and wear and tear on tactile sensor elements. Materials that cause wear, adhesion, or abrasion damage to measurement solutions such as measuring wheel encoders, impairing their function, can be measured by the SPEETEC® with a high degree of process reliability and availability.
Safe and highly accurate measurement principle
Since the SPEETEC® is equipped with class 1 lasers, it offers an alternative to expensive laser velocimeters and the associated costly protective measures. The return on investment (ROI) is particularly attractive. For the SPEETEC®, this is less than a year.
The non-contact measurement is performed with a laser Doppler process at speeds of up to 10 m/s. Two transmitters emit laser light – one in the direction of movement of the material, the other in the opposite direction. Since the transmitters work independently, possible mounting tolerances and surface fluctuations (i.e., with wavy surfaces) can be balanced out.
All measurements are done with high precision. At a resolution of four micrometers, the accuracy relating to the object length of a meter is one millimeter. The repeatability in this case is specified with a half a millimeter. Measured values are output via the TTL or HTL interfaces common in the encoder world, making integration easy.
Better productivity while saving resources
With the SPEETEC®, length, speed and position can also be detected in linear movements when switching between forward and backward motions. In addition, acceleration measurement in applications with high motion dynamics is possible since, with the SPEETEC®, only three milliseconds pass between the start of the movement and the output of measured values.
Comparable systems are much slower here. The speed sensor from SICK also creates new resource-saving solution options in the speed measurement of short materials. While velocimeters often require several meters of material feed, with the SPEETEC®, individual parts down to the size of a business card can be reliably measured.
Award-winning design: iF Design Award 2020
The rugged housing is designed for long-term use. Its shape and compact size characterize its high-quality design and enable integration into even the smallest spaces. The long window and the smooth edges indicate the measurement and mounting direction. These features impressed the judges of the iF Design Award. The SPEETEC® won the iF Design Award 2020 in the Product category.
About SICK
SICK is one of the world’s leading manufacturers of sensors, safety systems, machine vision, encoders and automatic identification products for industrial applications. With more than 1000 patents, SICK continues to lead the industry in new product innovations. The diversity of its product line allows SICK to offer solutions at every phase of production in the logistics, automotive, packaging, electronics, food and beverage, and material handling markets. SICK AG was founded in 1946 and has operations or representation in 65 countries worldwide.
Contact
Mandee Nguyen
SICK, Inc.
6900 W 110th St
Minneapolis, MN
55438 USA
Phone: 800.325.7425
Fax: 952.941.9287
Email: mandee.nguyen@sick.com