Configurable 2D and 3D machine vision solutions driven by SICK AppSpace

Jun 25, 2020

 MINNEAPOLIS, MINN., JUNE 24, 2020 – Easily create individual SensorApps on your own–without programming skills– to solve new automation tasks. Starting at the end of the year, this will all be possible in the SICK AppStudio, part of the SICK AppSpace ecosystem.

 

“Automation concepts are rarely standard”, explained Dr. Timo Mennle, SICK AppSpace Strategic Product Manager at SICK AG.
 
Even if you are supposedly dealing with a standard problem, additional configuration and customization work is required for many projects. These are details that could quickly result in higher costs and delays during installation. SICK customers can create their own individualized SensorApps to solve individual sensor applications — without having to program anything.
 
SICK AppSpace opens doors
 
In the SICK AppSpace eco-system, programmable sensors and edge devices can be configured for new tasks using SensorApps. Many apps are already available for download via the SICK AppPool. For specific applications, SensorApps can also be used independently by the customer and developed together with SICK experts and the support of a developer community. Until now, basic programming skills were required to generate your own SensorApps in SICK AppStudio. That is no longer the case with the new AppPool.
 
With a new graphic interface in SICK AppStudio, users can now solve specific sensor applications, even without programming skills, by configuring and linking pre-defined function blocks in a data flow. The starting point is always figuring out what the sensor has to do.
 
“If a customer wants to differentiate between and count deodorant bottles using the cap color, the cusotmer creates a data flow from function blocks existing in a library. After every step, a preview of the result is generated and the configuration can be adjusted right away,” said Mennle about the creation process.
 
Thanks to the open architecture of SensorApps, there is still the option of adjusting the source code of function blocks to implement more challenging applications and individual requirements.
 
New SensorApps for the AppPool
“By graphically processing data flows, we create the foundation for a larger target and user group. Then more users can take advantage of this for their applications,” said Mennle.
 
The rising demand for new and adapted function blocks can be satisfied from our growing community of developers. The diversity and possibilities of the SICK AppPool are growing, as are the fields of application of sensors and sensor systems.
 
FOR IMMEDIATE RELEASE
 
About SICK

SICK is one of the world’s leading manufacturers of sensors, safety systems, machine vision, encoders and automatic identification products for industrial applications. With more than 1000 patents, SICK continues to lead the industry in new product innovations. The diversity of its product line allows SICK to offer solutions at every phase of production in the logistics, automotive, packaging, electronics, food and beverage, and material handling markets. SICK AG was founded in 1946 and has operations or representation in 65 countries worldwide.

www.sick.com

Contact

Mandee Nguyen
SICK, Inc.
6900 W 110th St
Minneapolis, MN
55438 USA
Phone: 800.325.7425
Fax: 952.941.9287
Email: mandee.nguyen@sick.com