SICK's company history

When used in combination with precise optics and intelligent electronics, light can provide the answer to a wide range of issues. This potential was recognized quite some time ago by Dr. E.h. Erwin Sick, who set up his own company back in 1946. In the years that followed, Sick developed his company into a global provider of intelligent sensors and solutions for industrial automation technology.

    • SICK AssetHub
      2019

      SICK AssetHub: SICK AssetHub is a digital web service with which the digital twins of all devices or plants of a company can be managed, independent of manufacturer.

    • outdoorScan3
      2018

      outdoorScan3: The first of its kind worldwide: SICK presents the outdoorScan3, a safety laser scanner for outdoor applications.

    • AppSpace
      2017

      AppSpace: SICK AppSpace combines software and hardware and consists of two elements: the programmable SICK sensors and the SICK AppStudio, an application development kit for sensor applications.

    • InspectorP6x
      2016

      InspectorP6x: Image processing 4.0 - Programmable InspectorP6xx camera.

    • microScan3
      2015

      microScan3: The innovative safeHDDM® scanning technology provides the microScan3 outstanding robustness, even in dust and ambient light, and delivers high-precision measurement data. This increases productivity and machine availability.

    • GLARE
      2014

      GLARE: GLARE gloss sensors determine the gloss level of flat object surfaces and can differentiate between objects of different gloss levels.

    • Flexi Loop
      2013

      Flexi Loop: The unique, remote integration design of the Flexi Loop allows SICK to meet the demand for cost-saving cascading of safe switches and sensors within a machine.

      DeltaPac: For more efficiency and quality in the packaging industry: The DeltaPac multi-task photoelectric switch combines Delta-S technology®, two high-resolution energy scales, SIRIC® and distance measurement. The sensor detects object contours with radii of up to 20 mm regardless of direction thanks to the four operating modes that can be selected with a click.

       
    • GHG-Control
      2012

      GHG-Control: Measuring greenhouse gases instead of calculating them

      FLOWSIC500: The world's first ultrasonic compact gas meter for gas distribution.

    • EKS/EKM36
      2011

      EKS/EKM36: New motor feedback system with digital HIPERFACE DSL interface.

      MERCEM300Z: Advanced mercury monitoring system with improved sensitivity.

    • Color Ranger E
      2010

      Color Ranger E: The world's first high-speed 3D camera with high-performance color measurements.

    • Navigation basierend auf natürlichen Landmarken
      2009

      Navigation based on natural landmarks.

    • 2007

      High-end CCD sensor with integrated illumination.

    • Kleinster Sicherheits-Laserscanner
      2006

      Smallest safety laser scanner S300.

    • 2005

      IO-Link: Continuous communication through innovative sensor/actuator interface.

      RFID systems make it possible to identify objects without visual contact between reader and object to be identified.

    • Dreidimensionale Kamerasensoren
      2004

      3D camera sensors.

    • 2004

      First high-safety, camera-based safety system for presses.

    • 2003

      New generation of photoelectric switches: Sensor array with place- and time-triggered measurement of both the object to be detected and especially the environment.

    • 2002

       Proximity laser scanner with dynamic protective field switching for automated guided systems.

    • Hochgeschwindigkeits-2D-Codeleser
      2001

      High-speed 2D code reader. 

      Teach-in vision sensor.

    • 2000

      Miniature cylinder sensor.

      Safety bus system.

    • 1999

      First photoelectric switch for detecting light sections of a laser line on a 32 x 32 pixel field for determining the shape and position of objects.

      First budget photoelectric switch based on time-of-flight technology.

      First photoelectric switch with Teflon-coated housing for the electronic and process industry.

      First bar code reader with integrated autofocus based on time-of-flight technology.

      Smallest fully extrusion-coated magnet sensor

    • 1998

      First photoelectric proximity sensor which is insensitive to ambient light sources.

    • 1997

      SICK modular advanced recognition technology (SMART) makes it possible to identify even damaged bar codes.

      First contrast scanner with dynamic teach-in and high switching frequency.
       
    • 1996

      First time-of-flight device for positioning items in high-bay warehouses.

      First photoelectric switch with ambient light.

      First miniature photoelectric switch with background suppression.

      First application of a proximity laser scanner for volume measurement.

      First luminescence scanner in the field of automation technology with UV LED.

    • 1995

      First color sensor.

    • 1993

      First area scanner in safety category 3 for protecting hazardous areas.

    • 1991
      First use of area scanners for site security (e.g., when entering or leaving through lock gates and access points).
    • Erste Entfernungserfassung mit Laserlicht
      1989

      First distance determination with laser light on the time-of-flight of pulses principle.

    • 1986

       First in-situ diode array spectrometer for sulfur oxide, nitrogen oxide, and ammonia.

    • 1983

      Carbon monoxide measuring device for monitoring emissions in road tunnels.

      First use of printed code characters that can be scanned by laser scanners.
    • Erstes Volumenstrommessgerät
      1982

      First volume flow measuring device based on the ultrasound time-of-flight process.

    • 1978

      First in-situ gas measurement device for sulfur dioxide and nitrogen oxide (filter correlator).

      First photoelectric switch for detecting the position of a reflector by means of a four-fold reception element.
    • 1976

      First area scanner with V-shaped, rotating beam and special reflector in safety category 2 for protecting hazardous areas.

    • 1975

      Introduction of the semiconductor diode for the transmitter beam in photoelectric switches and proximity switches.

      First safety grid curtain for controlling protective hoods on eccentric presses.

      First color-ring code reader for detecting colored ring codes on ampules.

    • 1973

      Fiber-optic cable for detecting small objects when space is tight.

    • 1970

       First luminescence scanner for detecting luminophores in objects.

    • 1967

       Bar-code identification of packing lists, folding boxes, tins, tubes, etc. in the pharmaceutical industry.

    • 1964

      First curve control device for guiding a duplicating milling machine according to a construction diagram – the predecessor of today's NC milling machine.

    • 1962

      First optical height scanner for regulating filling levels.

    • 1960

      First weft winder monitor for very thin knitting thread (autocollimation principle).

    • optischer Zähler
      1959

      First rapid optical counter with display and integrated target value definition for quick detection of small objects.

    • 1956

      First optical-electronic flue gas monitor based on the autocollimation principle.

    • Unfallschutz-Lichtvorhang
      1952

       Static accident prevention light curtain with hollow mirror, without mirror wheel.

    • Nahtaster Sensor
      1951
      The NT1 close-range scanner:
      • A printed mark control device for the packaging industry
      • First light curtain for accident prevention on production machines
    • Skizze
      1950
      First practice-oriented photoelectric switches based on the autocollimation principle for industrial automation.
    • 2019
    • 2018
    • 2017
    • 2016
    • 2015
    • 2014
    • 2013
    • 2012
    • 2011
    • 2010
    • 2009
    • 2007
    • 2006
    • 2005
    • 2004
    • 2004
    • 2003
    • 2002
    • 2001
    • 2000
    • 1999
    • 1998
    • 1997
    • 1996
    • 1995
    • 1993
    • 1991
    • 1989
    • 1986
    • 1983
    • 1982
    • 1978
    • 1976
    • 1975
    • 1973
    • 1970
    • 1967
    • 1964
    • 1962
    • 1960
    • 1959
    • 1956
    • 1952
    • 1951
    • 1950
70 YEARS OF INNOVATION IN 612 SECONDS
SICK uses cookies

We use cookies to optimize our web pages for you, to continuously improve them, and to offer you information that is tailored to your interests. By clicking the “Accept all cookies” button you consent to the use of cookies. You can select which cookies you want to allow by clicking the “Show settings for cookies” button. For further information, please see our privacy policy.