Chemical Reactions? No thanks!

Jul 1, 2015
Gerd Kieper, Michael Markus, SICK Maihak GmbH, Reute, Germany

 

Abstract

The safety of various chemical processes and the supply chain can only be secured if they are kept under a controlled and modified gas atmosphere. Oxygen is often one of the unwanted gas components to consider. For example, during storage of flammable liquids or gases in tanks or their transport in pipelines, the removal of oxygen by inert gases is often needed to avoid flammable or explosive gas mixtures. For safety reasons, the integrity of the so-called inertization process must be insured at all times. The use of oxygen transmitters in or at the process devices is a suitable means to increase safety and efficiency in inertization processes. Affordable TDLS based oxygen transmitters have been recently introduced to the process market. They combine the technological advantages of a tuneable diode laser sensor with a simple transmitter design for a wide range of applications.

 

Introduction

 

To avoid any explosion, the operator of a process plant has the chance to eliminate at least one of the three basic properties belonging to the so-called ignition triangle. These are basically a fuel, an ignition source and an oxidizer. An explosion can only occur when all three items are coming together at the same time. What can be done to avoid this occurrence? Very often, chemical substances to be stored or transported for later use in a downstream process must be regarded as fuels. Ignition sources for example, an electrical spark introduced by a current source or a hot surface in the surrounding area cannot be easily eliminated without some effort and additional costs. Furthermore, the absence of any ignition source at any time is hard to maintain across the whole production area and it’s supply chain. The easiest way to reduce the risk of an explosion is through the reduction of the presence of any substance in the environment which can act as an oxidizer like the oxygen molecules in the ambient air. This can be achieved for example, by introducing a non-reactive gas, a so-called inert gas, to replace the air. Suitable inert gases are nitrogen, carbon dioxide, flue gases, and all noble gases. Consequently, the process to replace a potential oxidizing atmosphere by a non-reactive gas is called inertization.

 

Inertization Processes

 

The inertization of storage tanks, pipelines and/or process devices is not only used for preventing fire and explosions. It can also be applied to avoid unwanted chemical reactions, like product degradation, discoloration and undesired secondary reactions. Hence, the general target of inertization is either to eliminate oxygen in the environment or at least to reduce its concentration to an acceptable and safe limit. The safe area which needs to be established at any time to prevent a hazardous situation is defined as the lower explosion limit (LEL) and the upper explosion limit (UEL) of the fuel to be considered. LEL and UEL are the lower and upper limits of the fuel concentration range, which would allow flame propagation in the presence of air. A flame propagation cannot take place below or above LEL and UEL, respectively. In practical terms, a fuel mixture below the LEL is too lean to ignite or explode, whereas a mixture above the UEL will be too rich. The required limits are typically given in percentage range of volume or in g/m³ units.

 

The maximum oxygen concentration which can be regarded as safe is the so called limiting oxygen concentration (LOC). Therefore, the LOL value defines the maximum allowed oxygen level inside a mixture of a flammable gas, air and any inert gas constituents in which an explosion will not occur. The inert gas is either used to purge a vessel before filling it with the fuel or will be filled in as a safety or protective atmosphere above the product. Such a vessel can be a storage tank or a degassing silo, but also a chemical or pharmaceutical reactor, a centrifuge, a dryer, a mixer, a mill or any other equipment containing flammable material.

 

Inertization in practice

 

There are different ways to achieve a safe atmosphere or an inertization inside a vessel.

 

Vacuum inerting:

 

This is a common method for the inertization of vessels meant for vacuum operation. This procedure is normally not suitable for large storage tanks because they are usually not designed for vacuum conditions and can only withstand a negative differential pressure of a few mbar. The single operating steps include:

  • Create a vacuum in the vessel until a desired residual pressure is reached
  • Re-pressurize the vessel to atmospheric pressure with an inert gas, such as nitrogen

The steps are repeated until the desired oxygen concentration is reached.

 

Pressure inerting:

 

Vessels may be pressurized by adding inert gas, followed by venting to the ambient environment. More than one pressurization cycle might be necessary to reduce the oxygen content to the desired concentration. An advantage over vacuum purging is that the pressurization process is much faster. The disadvantage is that the process consumes more inert gas.

 

Flow through inerting:

 

In the flow-through purging process, a purge gas is introduced to a vessel at one inlet, and flushes the mixed gas inside the vessel at another outlet. This purging process is commonly used when the vessels or equipment are not rated for over- or under-pressure. The purge gas is added and vented at atmospheric pressure. The process can be expensive for purging large storage tanks as it consumes a large quantity of inert gas. Continuous inerting methods are used permanently or on demand, respectively. Fixed-rate inertization requires a continuous feeding of the inert gas into the enclosure at a constant rate and results in a corresponding release of a mixture of inert gas and flammable gas from the vessel's head space. To ensure that the vessel is completely protected, the flow rate of the inert must be sufficient to satisfy even peak-demand requirements.

 

Siphon inerting:

 

The siphon purging process starts with filling the vessel (e.g. a large storage tank) with a liquid, such as water or any other non-flammable liquid compatible with the product. The purge gas is subsequently added to the head space of the vessel and drains the liquid from the vessel. When using the siphon purging process, it may be desirable to fill the vessel with the liquid first and then use the flow-through purge process to remove any oxygen from the residual head space.

 

Displacement inerting:

 

A method based on density differences between the inert gas and the gas which has to be replaced. Ideal replacement happens when a stable horizontal interface exists between the lighter gas entering at the top of the tank and the heavier gas at its bottom through some suitable piping arrangement. As it is important to achieve the required degree of gas replacement throughout the full tank cross section this method requires a relatively low entry velocity of the gases and more than one complete volume change to ensure the inertization.

 

 

Inertization surveillance

 

Several methods exist to control these different inerting methods in a reliable way, including pressure, flow and oxygen monitoring. In the flow monitoring mode, the flow rate of the inert gas supplied to the vessel is regulated whereas in pressure monitoring mode the vessel pressure is controlled. Decreasing vessel pressure will be compensated by increasing the amount of inert gas, whereas a pressure rise inside the vessel might result in venting inert gas from the vessel into the ambient.

 

Oxygen monitoring is the only method of all the ones mentioned, where the gas composition of the inert atmosphere is controlled in a proper way. With the help of oxygen monitoring, the accurate adjustment of the allowable oxygen concentration can be made to the required level within the fuel-gas-mixture. Therefore, oxygen monitoring provides a dynamic and flexible control of every inertization process. Oxygen transmitters can be installed either directly into the inert gas generating system, e.g. nitrogen generators, into the inert gas supply stream or directly into a vessel or pipeline, on the spot where undesirable reactions should be prevented.

 

Because the integrity of the intertization must be secured along the whole process the use of oxygen transmitters at any of these locations is recommended. This results in a cost efficient control of the inerting process and speeds up the reaction time in case of any unforeseen changes or malfunctions of a process device. The task for an oxygen measurement in the context of intertisation applications might be also the safety of the staff, operating these processes. Potential leakages of the inert gas generator, pipeline, or vessel during operation or maintenance could result in an oxygen deficiency in the surrounding atmosphere and can in the worst case lead to suffocation. Hence, it is worth considering oxygen monitoring also in the environment around the intertization processes.

 

How to find the right oxygen sensor?

 

Several oxygen sensor technologies are available in the market promising a reliable and safe solution for the applications mentioned above. In general, if they are chosen with care all of them could be used at some of the measurement points along the described inertization processes and in their periphery. Here, the user’s expectations in terms of performance, reliability and lifetime cost of the sensor equipment will make the difference. All types of oxygen sensors have their advantages and disadvantages. Limitations for the individual sensor technology are shown as follows:

 

Oxygen analyzers based on electrochemical sensors are the most known technology to measure oxygen in the ambient or in process gases. The sensor resembles an electric battery and consists of a cathode and anode with an electrolyte (mostly acetic acid) in between. A red-ox reaction, initiated by the presence of oxygen ions, results in an electric current which is measured to determine the oxygen concentration in the surrounding gas. The big advantage of this measuring method is the wide range of concentrations which can be measured (ppm-level … 100%O2). It is found very often in small portable analysers used for operator protection. The disadvantage of this measurement method is the finite lifetime of the sensor which can vary between six months and three years depending on the actual measured oxygen levels. These sensors tend to drift heavily. A frequent calibration - at least once a month - is needed to compensate these drifts. Additionally, electrochemical sensors have only a very limited tolerance to harsh chemical environments.

 

Zirconium Oxide (ZrO2) based sensors detect the difference in the oxygen content in a known gas composition (e.g. reference air) and in the measuring gas by the resulting voltage drop according to the Nernst equation. The voltage drop gets higher with increasing difference in the oxygen concentration in the reference gases and in the measuring gas. This sensor is ideal for measurements in ppm-range but can be also used up to 100% oxygen level. It has fast response times and good accuracy. Disadvantages are the relative short lifetime of the sensor (approx. 18 months), the high power consumption and the cross-sensitivity to hydrocarbons, CO, H2 and other combustible gases. Condensates will directly destroy the sensor.

 

Measurement principles based on the paramagnetic properties of oxygen molecules are very often used, especially in the context of inertization in the process industry. Applicable for relatively high oxygen concentrations in the %-level, the sensor utilizes a strong magnetic field to detect the oxygen molecules inside a sample gas. The analyzer works reliably and is  stable only in connection with a proper sample conditioning system. It has a good selectivity, but the sensor is quite expensive and sensitive to pressure fluctuations, flow drifts, vibrations and gas impurities like humidity and dust. An in-situ design is not available.

 

Tuneable Diode Laser Spectroscopy (TDLS) often used for oxygen detection is well known for its selectivity and stability but also for its high cost. Until now, oxygen analyzers based on TDLS are mostly used for rather difficult process measurements in the chemical and petrochemical industry or for combustion control of incinerators. Typical installations include two flange-mounted units, one acting as a receiver and the other as the transmitter. Therefore, beam alignment is often required as well as inert gases e.g. nitrogen to purge the dead volume close to the mounting flanges. A big advantage of the TDLS technology is the ability to measure under hard environmental conditions, e.g. high temperatures, corrosive gases, etc. TDLS technology would be the optimum for all measurements, but have often been disregarded as not affordable for standard applications.

 

A new TDL based oxygen transmitter on the market provides a reasonable and very cost efficient solution which combines the unique properties of the TDLS technology with the simplicity of a process transmitter. The product is designed for harsh ambient conditions and can be mounted either directly to a process vessel or a gas pipe as an in-situ sensor or, if the process conditions do not allow this, in a simple by-pass configuration using an optionally available sample cell. Also available as an option is a wall mounting bracket which allows for installation close to the measuring point or as an ambient air monitor for oxygen deficiency monitoring. Available is a general pupose version or an FM certified one for hazardous areas. (ATEX version will follow).

For the inertization process described, the unique TDL based oxygen transmitter offers an excellent long term stability (a calibration once a year is recommended) and the absence of any moving or wearing parts. The sensor parts in contact with the process media are protected by a fine steel mash filter and by an optional PTFE membrane. In any case, the optical parts can be easily cleaned, as well. The analyzer tolerates aggressive chemicals and moisture. There is no need for an additional reference or purging gas. Important for inertization processes: hydrocarbons do not interfere with the measurement. The product is the first TDL based transmitter at a price which is reasonable for a wide range of oxygen monitoring applications. As a consequence, TDL based oxygen transmitters can make inertization processes safe, reliable and cost efficient at a minimum of investment and lifetime costs.

 

 

 

Figures:

Fig 1. Ignition Triangle (Picture not licensed! Perhaps you can fill in something similar.)
Fig 1. Ignition Triangle (Picture not licensed! Perhaps you can fill in something similar.)
Fig. 2. The TDL based oxygen transmitter TRANSIC100LP
Fig. 2. The TDL based oxygen transmitter TRANSIC100LP
Fig.3 General pipeline picture
Fig.3 General pipeline picture

 

SICK is one of the world's leading manufacturers of sensors and sensor solutions for industrial applications. Founded in 1946 by Dr.-Ing. e. h. Erwin Sick, the company is headquartered in the German town of Waldkirch, in the Breisgau region near the city of Freiburg. It is a technology and market leader, maintaining a global presence with more than 50 subsidiaries and equity investments as well as numerous representative offices. In the 2014 fiscal year, SICK had around 7,000 employees worldwide and generated Group revenues of €1,099.8 million.

Download

IAA_O&G_052012