For Increased Efficiency, Deep Learning is the Future

Jan 16, 2020

Machines are learning to think. Deep learning is a machine learning technique − and the most significant future technology in artificial intelligence. SICK transfers this key technology to its sensors, offering customers added value for greater productivity and flexibility.

Computer screen with deep learning
Computer screen with deep learning

If greater efficiencies are to be made at each stage of production, clever machines must adapt. Logistics process automation is continuing to gather momentum. Interest in intelligent machine behavior is increasing, and with it, the challenge of digital technology. Sensors remain the source of information, and integrated software offers a solution for evaluating and communicating networked data. However, the Industry 4.0 trend means there is an urgent need for “reformed” thinking in IT on data complexity. Deep learning is essential and it’s the path SICK and its customers is taking for modern plant processes.

 

Deep learning thinks like a human

Deep learning requires algorithms capable of detecting and processing vast, complex amounts of patterns and data. The artificial neural network mimics human thinking and learns from examples. It learns from experience and learns to adapt to new, updated information. As a result, a range of optimizations are possible today that would have been unthinkable just a few years ago. Machines and plants, in combination with intelligent data and specialized sensors, can find solutions to the most complex tasks. 

 

Reality check

Most of SICK’s current deep learning projects are in the field of optical quality inspection. In logistics automation, deep learning cameras can automatically detect, verify, classify, and localize “trained” objects or features by analyzing the taught-in image base. For example, they can check whether any flats are present in the sorter trays, optimizing sorter cell assignment and increasing throughput. They detect strapping bands on parcels − even white bands on white parcels. This improves quality control in the automatic packaging process and makes sure that transported objects are analyzed. If packages are dented or damaged, or if the material properties of the parcel need to be determined, SICK sensors can intelligently capture and evaluate structures or features during live operation. They ensure that the next steps in the sorting process are initiated. This feature is unique in this form and could previously be performed only by the human eye. The ultimate aim of all SICK projects is to apply deep learning to improving processes and increasing plant effectiveness.  

deep-learning-in-logistics-out-of-the.box
deep-learning-in-logistics-out-of-the.box

Top specialists, complex algorithms, high computing power

The demand is not for a universal solution. Rather, the focus is on a solution tailored to a specific case. Although modern 2D and 3D cameras are becoming ever faster and more powerful, their performance is currently restricted by traditional image processing algorithms. In order to assess different applications and conditions, SICK’s deep learning experts work closely with the client’s process and quality experts. Their unique process expertise forms the basis of simulation training and the heart of subsequent deep learning algorithms in the sensor. 

A complex network architecture processes the enormous quantity of information. In spite of this, the time needed to train a deep learning network comes to little more than a few hours. Deep learning networks can also be retrained and adapted to new conditions. For big data pools and neuronal network training, SICK uses powerful independent, internal processing and IT systems. The deep learning algorithms generated are placed on the sensor locally via the cloud, making them fail-safe and directly available on an intelligent camera. 

There’s still a long time to go before machines truly reign supreme, yet even today, deep learning is achieving impressive results and offers many benefits. The essential work, however, is still being done by humans. Only time will tell how many companies and industries will decide to fuel their growth by stepping up their investment in this digital technology. Be a part of the revolution − with new projects. With SICK.  

 

 

SICK使用Cookie

我們使用Cookie為您呈現最佳的網站設計,持續改進網站並向您提供您感興趣的客製化資訊。 確認「同意全部Cookie」按鈕即表明您同意我們使用。 透過「顯示Cookie設定」按鈕可以選擇允許使用何種Cookie。 其他資訊可在資料保護聲明中查閱。.