Victorian British industrial history met state-of-the-art 21st Century digitilisation from SICK to deliver a surprising sensing solution high in the windy moors of West Yorkshire.
When Wayne’s Water World Went Digital…
But climate change and increasing demand is putting the historic facility under stress. So, the SICK sales consultant enlisted his colleague Charlie Walker, the company’s UK digital product manager, to make sure a continuous water supply to residents could be maintained. The solution took not just 21st Century know-how, but plenty of 19th Century-style hands-on Northern hard graft.
Historic Water Facility
Water Stress
![](https://cdn.sick.com/media/content/hc3/h1a/13523566133278.jpg)
Digital Solution
![](https://cdn.sick.com/media/content/hfa/h34/13523571736606.jpg)
Charlie and Wayne installed a SICK CFP level sensor in the tank, and SICK FTS flow meters to monitor the flow on the outlet pipe to the village. Water from the tank is gravity fed down the 0.5km pipe to a treatment plant on Henshaw Road.
The solar and wind power generation has a combined capacity to pull up to 3 amps and 150m of cabling also had to be installed.
“Data collected from the SICK FTS flow meters can also be used with the level measurement to calculate any water loss in the system. None of this additional data would be available without a digital system, or even just installing a single sensor with an on-device display.”