Forklift safety: all the technologies to protect workers

Nov 8, 2023

Handling products in Industrial enviroments requires maximum precision. This is the reason why SICK develops safety solutions for forklifts. 

Efficiency and productivity on the factory floor are crucial. That is why awareness of potential hazards in production and logistics environments is essential. One example is forklift trucks: their size and “mobile" nature makes them potential sources of accidents. There can be many causes: distractions or lapses in concentration on the drivers' part, as well as speed and the amount traffic due to busy work schedules.

Although no specific data is available on forklift accidents, the statistics give us an insight into the importance of safety on the factory floorEurostat data shows that in 2020, non-fatal accidents in the manufacturing sector accounted for 18.6% of all accidents in the EU, while fatal accidents accounted for 15.2% of the total. 

Automation technologies can help companies improve the safety of employees when they are working in environments where forklifts operate. Sensors, for example, are able to support operators with solutions that ensure high safety of movement, precise positioning, and position recognition. 
 

H2: Forklift safety: Backup Assistance System 

An example of a forklift safety system is the SICK Backup Assistance System (BAS), which generates alerts when a vehicle is in close proximity to a person or object to help drivers avoid accidents. This is especially important in cases of reduced vision, such as blind spots or during reversing manoeuvres. BAS is a stand-alone system that doesn't require reflectors or transmitters and is an ideal solution for ensuring targeted coverage of known blind spots as well as optimising the coverage of the side areas, where the driver's view is reduced. 
 
The Backup Assistance System provides a warning signal when an obstacle is detected. The system comprises one or more TiM351 LiDAR sensors, a control unit, a light bar, and an audible alarm. 
 
The LIDARs can be installed on the rear of the forklift or attached to the side of the vehicle to increase visibility. The area to be monitored can be scaled and easily adjusted. The Backup Assistance System is also characterised by low power consumption, which minimises the vehicle's battery consumption. 
 

H2: Forklift safety: Drive Assist System 

The SICK Drive Assist System (DAS) is a collision avoidance system for forklift safety. It can be integrated directly by the vehicle manufacturer into the control unit, and it is also possible to implement a customizable warning function or dialogue directly with the vehicle control unit. In this way it is possible, for example, to reduce the vehicle's speed or stop it. 
 
The system allows the implementation of integrated warning strategies for anti-collision function and driver support. The detection of the environment is 270 degrees and can be specifically adapted to the use of the vehicle. Distances between vehicles and objects can be determined precisely for the protected area thanks to the sensor output which provides distance values in polar coordinate from predefined sectors. 
 
Object detection is reliable and independent of shape or surface, even in environments with intense ambient light. Smart data pre-processing takes place directly on the sensor, thus avoiding the need for additional hardware or software. 
 

H2: Forklift safety: solutions for pick and place applications

Forklift safety is not only relevant for movement inside or outside the factory. Pick and place operations can also pose a danger to operators. SICK's inductive proximity sensors from the IME and IMB series enable the precise detection of fork positions so that information can be presented to the operator conveniently on a display. 
 
Finally, to allow fork height measurement and detection of lateral movements the SICK linear encoder EcoLine can be integrated into the lifting frame. This enables automatic pre-adjustment with different pallet sizes.
SICK uses cookies

We use cookies to optimize our web pages for you, to continuously improve them, and to offer you information that is tailored to your interests. By clicking the “Accept all cookies” button you consent to the use of cookies. You can select which cookies you want to allow by clicking the “Show settings for cookies” button. For further information, please see our privacy policy.