The sensitivity of grippers and gripper arms is becoming increasingly important, especially when it comes to flexible production and batch size 1. Intelligent object detection is the key to complex automated applications. Light sources and detection functions can be customized and preset in line with special object properties relating to material, surface, or form, for instance. The intelligent sensors from SICK cover all applications for End-of-Arm Tooling and the respective feed systems.
Selection of robot applications for End-of-Arm Tooling
Our products and solutions for End-of-Arm Tooling
Practical examples – stories in the SICK Sensor Blog
SICK sensors controll pharmacy robot
Finnish company Capps Oy has developed an automated storage system for pharmacies that is based on completely new thinking. The machine takes only a fraction of the space of traditional storage but can hold many more products.
![](https://cdn.sickcn.com/media/content/hd5/hbe/11111841202206.jpg)
Do you have any questions?
Specific solutions for leading robot manufacturers