Privacy policy of a collision avoidance system

SICK le agradece su visita a nuestras páginas web y su interés por nuestra empresa, nuestros productos y nuestros servicios. La protección de su esfera privada es de gran importancia para nosotros y esperamos que se sienta seguro durante su visita a nuestras páginas web. Por este motivo deseamos explicarle a continuación qué información tratamos durante su visita a nuestras páginas web.

Responsible SICK AG, Erwin-Sick-Straße 1, 79183 Waldkirch, Germany
Purpose of processing Development and validation of a collision avoidance system
Categories of data
  • Image data
  • Video data
  • 3D information
  • Geoposition data
  • Time of recording
  • Weather data
The quality of the video material only allows people to be identified if they are within 3.8m of the camera.
Legal basis GDPR Art. 6 (1) f) - legitimate interests
Legitimate interest SICK processes images and videos in combination with time, geoinformation and weather data for the training and validation of AI systems. Most of the data is processed automatically. This processing is done to protect people in the vicinity of machines and to prevent accidents involving them.   By developing such a system for the protection of persons, there is a justified company interest in the general welfare of all persons. Due to the purpose of the system's accident prevention, the future protection in the interest of all people therefore outweighs the right to the image recordings of the individual, which is worthy of protection.
Consequences of failure to provide the data The data is provided fully automatically via the recording system.
Retention time As a product to be classified as a high-risk AI system in accordance with EU AI Act Article 6 is also to be developed on the basis of this data, it is necessary to store the data. Based on the data, the accuracy and robustness of the product is to be evaluated and improved throughout the product life cycle. In order to safeguard product liability in accordance with Section 13 (1) ProdHaftG, the recorded data is stored for 10 years after the last sale of a system based on this technology. 
Data source We process data generated by the recording system.
Recipients of the data Certifying bodies
Transmission in third countries We do not transfer any personal data to third countries.
Logic of the automated decision We do not make automated decisions.

 

Sus derechos

Ud. tiene derecho a

  • la información sobre sus datos personales;
  • la rectificación de sus datos personales;
  • el borrado o bloqueo de sus datos personales;
  • la oposición al tratamiento de sus datos personales;
  • la portabilidad de sus datos personales;
  • la revocación de su consentimiento con efecto futuro si el tratamiento de sus datos personales se basa en su consentimiento; así como a
  • la reclamación ante una autoridad supervisora de protección de datos si considera que el tratamiento de sus datos personales viola la ley de protección de datos.

Diríjase para ello a nuestros responsables de la protección de datos. Responderemos adecuadamente a todas sus preguntas.

Modificación de la declaración de protección de datos

Nos reservamos el derecho de adaptar en cualquier momento esta declaración de protección de datos a los requisitos legales en vigor. La versión más actualizada de nuestra declaración de protección de datos se encuentra siempre disponible en nuestras páginas web.