Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.
609 results:
Result 289 - 312 out of 609
In the Netherlands, natural gas is a key source of energy and accounts for nearly half of the total energy mix. As we enter a new era in terms of energy, an intelligent approach to gas production is crucial...
Read on
Fitness or health apps read data from fitness wristbands or smartwatches and provide information about the current performance of the user. The apps also provide additional services such as digital manuals...
Read on
For Industrieservice Schach, working with SICK as a one-stop supplier is paying dividends both technically and financially. Based in Nürtingen, Germany, the company uses state-of-the-art sensor technology...
Read on
Goods flows multiply for Christmas business, and logistic systems face major challenges every year - in production and trade, as in the area of dispatch services. The final link in the logistical chain,...
Read on
Costly manual measurement of raw chipboard is a thing of the past. The SicoCam inline board measurement system from Siempelkamp Logistics & Service now measures wooden composite boards in a continuous...
Read on
Managing the future with "Sensor Intelligence.": At SPS/IPC/Drives 2017, SICK once again presented exciting trends and innovations. During recent years, digitalization and networking in production...
Read on
Especially when it comes to Industry 4.0, integration capability and consistency are important features of intelligent and future-proof communication structures. That is why SICK offers several options...
Read on
At SICK, sensor data travels by bus: Fiber-optic sensors and distance sensors are connected to a WI180C-PB fieldbus module and integrated in PROFIBUS systems. The communication module enables quick access...
Read on
Fully-automatic watering systems, placing robots for the potted plants, climate computers for perfect ambient conditions or picking of different plant types. The flower industry now uses automated high-tech...
Read on
A garbage truck driver is faced with challenges on a daily basis, including illegally parked cars, narrow roads, irritated motorists, heat, cold, and thunderstorms. It does not have to be like this any...
Read on
Small, but a global leader all the same: Ehrler Prüftechnik Engineering GmbH (EP-E) has crafted a remarkable reputation in the field of high-precision testing and calibration systems. A preferred...
Read on
Automated guided vehicles (AGVs) and automated guided vehicle systems (AGVSs) play a major role in increasing the flexibility of production and logistics processes. Used individually or in groups, these...
Read on
The rapid pace of progress in electronics and sensor technology is determining the level of innovation in mobile machines today. The manufacturers and users of agricultural and forestry, construction and...
Read on
Wanna bet that ... you can use an excavator shovel to place the tone arm of a record player precisely between two songs on a record, or hang up six socks with two excavators in the space of four minutes?...
Read on
Multimillion-dollar damage that occurs during aircraft ground handling leads to high insurance payouts every year. As a result, ground handling services are encumbered with higher insurance premiums.
In...
Read on
Agricultural machines are exposed to extreme situations which require a high degree of ruggedness to withstand. Only the tough - and the giving - prevail. IMB inductive proximity sensors make a major contribution...
Read on
The Old City Harbor of Tallinn is one of the busiest on the Baltic Sea. The wish to control the steadily increasing traffic volume and to improve the experience for passengers has prompted the port operator...
Read on
Now there is no need to go without ultrasonic precision and fall back on other mechanical measurement techniques in the event of a mains voltage failure. The back-up batteries in the FLOWSIC-X gas flow...
Read on
With mobile machines, accidents often occur when maneuvering and backing up on construction sites, in surface and underground mining, and in agriculture and forestry, as well as with special and municipal...
Read on
Delayed, damaged or lost baggage is more than just a nuisance. It reduces customer satisfaction and constantly generates costs. The IATA Resolution 753, which will soon come into force, is to change all...
Read on
Driver assistance systems based on 3D LiDAR sensors (also 3D laser scanners) or 3D vision sensors from SICK reliably detect blind zones around mobile machines and warn the operator of potential sources...
Read on
Selecting the right method and appropriate device for the flow measurement generally involves a time-consuming and resource-intensive consideration of the advantages and disadvantages of the different...
Read on
As Johann Wolfgang von Goethe once put it himself, sowing is not as difficult as reaping. Since then, much has changed owing to the motorization and mechanization of agriculture. And yet, harvesting crops...
Read on
It is clearly evident that digitalization has left its mark on the paper industry. Does "the print media” face an uncertain future or will haptic page turning hold its own? – both theories...
Read on
Result 289 - 312 out of 609
Please wait a moment...
Your request is being processed and may take a few seconds.